I am currently using Windows 7 64 bit; KSD 3.0 and can't resize the project generator window to reach the generate button. 

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I am currently using Windows 7 64 bit; KSD 3.0 and can't resize the project generator window to reach the generate button. 

跳至解决方案
4,995 次查看
jberri
Contributor II

I am currently using Windows 7 64 bit with KSD 3.0 and can't resize the project generator window to reach the generate button.  How can I take care of this problem?

标签 (1)
1 解答
4,682 次查看
adyr
Contributor V

Hi,

Check out the Windows DPI setting in "Control Panel\All Control Panel Items\Display" and make sure it is set to "Smaller -  100%". If the text on the screen looks to small after that change then change to a lower screen resolution. Unfortunately many modern displays have resolutions far higher than the physical screen size allows us to see so Microsoft allow us to try and upscale all the contents. However, this fails on many applications.

Best regards,

Adrian.

在原帖中查看解决方案

15 回复数
4,682 次查看
hiansuanchew
Contributor I

Have you found the solution? I have the same problem, and I have the same OS and monitor resolution like  yours. Can't find any answer from google

0 项奖励
回复
4,682 次查看
berthoboman
Contributor II

Unfortunately neither I nor Iva have found a solution to the problem.  It is "encouraging" that I am not alone with some defective hardware.

Hopefully someone will figure out why it is not working properly.

0 项奖励
回复
4,683 次查看
adyr
Contributor V

Hi,

Check out the Windows DPI setting in "Control Panel\All Control Panel Items\Display" and make sure it is set to "Smaller -  100%". If the text on the screen looks to small after that change then change to a lower screen resolution. Unfortunately many modern displays have resolutions far higher than the physical screen size allows us to see so Microsoft allow us to try and upscale all the contents. However, this fails on many applications.

Best regards,

Adrian.

4,682 次查看
berthoboman
Contributor II

Great info Adrian!

Changing the display to "small" will display the window properly.

At least I can use the program until it gets properly fixed so it also works with the medium and large display settings.

Thanks again.

4,682 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Jairo,

can you show us the problem (attach screenshot) are you facing?

I also use Win7 64bit and on my side is without problems:

ksdk.png

Thank you,

Iva

0 项奖励
回复
4,682 次查看
jberri
Contributor II

Thank you Iva for a very fast response.

Here is a screen capture:

Proj-Gen.png

The same executable works OK on another Win-7 -64bit.

The problem is on a Lenovo laptop.  I have been switching screen resolutions but no improvements.

0 项奖励
回复
4,682 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello Jairo,

please, what is your screen resolution?

Please, try this option for the application:

  • Right click on the application and choose Properties

ksdk_1.png

  • in tab Compatibility please choose resolution 640x480

ksdk_2.png

  • execute the application again

Please, let me know, if it helps you.

Iva

0 项奖励
回复
4,682 次查看
jberri
Contributor II

Thanks Iva,

I tried the 640x480 earlier.  The screen looked horrible but the problem iwa the same.

I have also tried changing the screen resolution but it did not help.

I have a dual monitor setup and dragging it to the other monitor does not help.

Bertho

0 项奖励
回复
4,682 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello Jairo.

Never mind, please what screen resolution do you use? It could help me.

Thank you.

Iva

0 项奖励
回复
4,682 次查看
jberri
Contributor II

Hi Iva,

The normal resolution is 2560 x 1440.

I have tried setting the system to lower resolution but no improvement.

Bertho

0 项奖励
回复
4,682 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Jairo,

please, have you already solved your issue?

Please check the option Smaller.

smaller.png

Thanks.

Iva

0 项奖励
回复
4,682 次查看
jberri
Contributor II

Thanks for checking.

Adrian's suggestion temporarily resolves the problem but of course it makes a mess of all the icons on the desktop.

Hopefully the development team will fix the bug by monitoring the resolution setting so this issue disappears.

Thanks again for you help.

4,682 次查看
ivadorazinova
NXP Employee
NXP Employee

I reported to SW team, so it will be fixed in next version.

I will let you know.

Best Regards,

Iva

0 项奖励
回复
4,682 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello Jairo,

ok - I try to come up with any workaround.

I will answer you as soon as possible.

Iva

0 项奖励
回复
4,682 次查看
berthoboman
Contributor II

Hi Iva,

Any success finding a solution to the problem?

Have a great weekend.

Jairo

0 项奖励
回复