How to install sdk2.0 w/ KDS 3.2 on Win7? Target board is TWR-KV58F220M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to install sdk2.0 w/ KDS 3.2 on Win7? Target board is TWR-KV58F220M

1,193 Views
fzhang1
Contributor I

I have downloaded the SDK builder generated SDK2.0 package for Windows, which is a .zip file. There is no .exe executable file inside the .zip package. How can I follow the SDK1.x instructions to install the SDK? The target board is TWR-KV58F220M. The Kinetis Design Studio 3.2 is installed already. Need some help here. Tried to use the Help->Install New Software menu item in Kinetis Design Studio, and run the Add button to point to the extracted SDK 2.0 folder after unzip the SDK2.0 package, and there was an error complaining the extracted SDK folder is invalid. I am lost here. Perhaps there are missing files in the generated SDK2.0? or I am not installing in the correct way?! Need some help here. Appreciated.

Frank

Labels (1)
0 Kudos
Reply
2 Replies

1,021 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Frank,

Please refer to https://community.nxp.com/docs/DOC-329662 

Hope it helps

Alice

0 Kudos
Reply

1,021 Views
fzhang1
Contributor I

Hi Alice,

Thanks for the response. It fixed the problem.

Frank

0 Kudos
Reply