GPIO output with frdm-kl43z and processor expert

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO output with frdm-kl43z and processor expert

983件の閲覧回数
christopherira
Contributor III

Hi,

 

I'm using the frdm-kl43z board and trying to control a simple output with processor expert.

I am able to do so with the on board LEDs, but when trying to output a voltage with the pins, I can't toggle an output.

I've configured several pins in processor expert but get nothing out.

 

these are the configurations of LEDs and J2_17:

133749_133749.pngpastedImage_1.png

I've also tried an output logic of 1 and various combinations of slew rate and drive strength.

 

This is my code to control a simple toggle of the output with the on board buttons.

133748_133748.pngpastedImage_0.png

It works fine with the LEDs but not with the Pins.

 

Thanks!

Chris

ラベル(1)
0 件の賞賛
返信
1 返信

813件の閲覧回数
christopherira
Contributor III

I realized that the pins are outputting 3 V, but they are not outputting enough current to power my air compressor.

Is there anyway to draw more current from the kl43z pins?

0 件の賞賛
返信