FreeRTOS for MKL16z128VFM4(FRDM KL-26Z)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeRTOS for MKL16z128VFM4(FRDM KL-26Z)

2,141 Views
vipinkumar27
Contributor II

Hi,

 

I am using FRDM KL-26z board for MKL16z128VFM4 processor.I am using KSDK v 1.3.0 mainline. I want to use FreeRTOS but I couldn't find the FreeRTOS example or even ,when I opened  Processor expert ,in OSs folder,I couldn't find FreeRTOS .c files.Am I using the correct KSDK ? I am not able to find the way out to FreeRTOS usage in KL26Z.

Labels (1)
0 Kudos
25 Replies

1,357 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Vipin,

You  can download and install the KSDK2.0, after install , you can find the FreeRTOS demo

as these:

pastedImage_0.png

About the detail method to download and install please refer to :

How to: install KSDK 2.0

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,357 Views
vipinkumar27
Contributor II

Thanks a lot.:smileyhappy:

0 Kudos

1,357 Views
vipinkumar27
Contributor II

Does it support MKL16z128VfM4?

0 Kudos

1,357 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Yes,

pastedImage_0.png


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,357 Views
vipinkumar27
Contributor II

Hi,whenever I am pressing Select Configuration after selecting Board-FRDMKL26Z,its not moving forward and returns back to the same page without any error.I tried it randomly by selecting other boards too but  same is happening .

Is there any other way to get ksdk2.0 for FRDM -KL26Z ?

0 Kudos

1,357 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Vipin,

Please take a screenshot about your process and the error , thank !

BR

Alice

0 Kudos

1,357 Views
vipinkumar27
Contributor II

Screen Shot 2016-02-22 at 2.33.54 PM.pngScreen Shot 2016-02-22 at 2.36.52 PM.pngScreen Shot 2016-02-22 at 2.37.29 PM.pngScreen Shot 2016-02-22 at 2.38.08 PM.pngScreen Shot 2016-02-22 at 2.38.29 PM.png

0 Kudos

1,357 Views
vipinkumar27
Contributor II

1st page-Download clicked.

2nd page-Kinetis SDK Builder Download clicked.

3rd page-Build an SDK clicked

4th page-Select Config after selecting FRDM KL26Z

5th page-the same page everytime not moving forward

0 Kudos

1,357 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Vipin,

please what browser do you use?

BR,

Iva

0 Kudos

1,357 Views
vipinkumar27
Contributor II

Google chrome but I tried with Internet Explorer and the same thing happened

0 Kudos

1,357 Views
ivadorazinova
NXP Employee
NXP Employee

Thank your feedback, I will report it.

Please, try it in Firefox, it works without problems.

Please, let me know if it works you.

Best Regards,

Iva

0 Kudos

1,357 Views
vipinkumar27
Contributor II

It is not working in Mozilla too.

0 Kudos

1,357 Views
ivadorazinova
NXP Employee
NXP Employee

Please, what do you use for the Firefox version?

You can use for this What browser am I using? Is my browser up to date? Web browser detection, Javascript, Cookies, Flash...

Best Regards,

Iva

0 Kudos

1,357 Views
vipinkumar27
Contributor II

1 week back,I had downloaded some Ksdk version by building the SDK and this thing was working even in google chrome.

0 Kudos

1,357 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Vipin,

thank you for the information.

The bug is reported Jira ticket KEX-797

Best Regards,

Iva

0 Kudos

1,357 Views
vipinkumar27
Contributor II

Can you please share the link for the repository of this file?

Email-id:vipinkumr27@gmail.com

0 Kudos

1,357 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Vipin,

we have been working on the issue.

But it is strange that you face the issue also in Firefox 44. I have installed Firefox 44 and it works for me on my side.

Yes, I have share it with you, but FRDM-KL26Z (MKL16Z128xxx4) is supported by KSDK 1.3 not by KSDK 2.0.

Best Regards,

Iva

0 Kudos

1,357 Views
vipinkumar27
Contributor II

I randomly tried downloading for other boards too but the KSDK2.0 wasn't getting download for anyone of them

0 Kudos

1,357 Views
vipinkumar27
Contributor II

I want to use FreeRTOS for my coding but couldn't find enough examples in KSDK1.3 and as per the discussion ,I thought KSDK2.0 is supported by KL-26Z.

0 Kudos

1,357 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Vipin,

there are a lot of examples, but not all of them are for your board.

Please, take a look at demo I2C RTOS located under C:\Freescale\KSDK_1.3.0\examples\frdmkl26z\demo_apps\i2c_rtos\i2c_rtos_freertos

I hope this helps.

Iva

0 Kudos