FreeRTOS LwIP SDK v2.0.0/V0.8.2 tpcipecho demo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeRTOS LwIP SDK v2.0.0/V0.8.2 tpcipecho demo

2,290 Views
李月鑫
Contributor I

Dear all,

  When implementing FreeRTOS lwip function on the basis of SDKV0.8.2 or V2.0.0 routines, we found that ehternetif.c file had no actual content, and compiled after changing #if 0 to #if 1, there were a lot of mistakes. Are there any people who have implemented TCP or other ping? Can resources be Shared/.

Best Regards

Labels (1)
Tags (1)
0 Kudos
Reply
5 Replies

2,149 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Yuexin:

This file is for MAC filters actions for IGMP and MLD6, it is from LwIP stack.   We don't have a plan to port IGMP to SDK at the moment.

Regards

Daniel

0 Kudos
Reply

2,149 Views
李月鑫
Contributor I

Hi,Daniel_Chen:

Based on the above situation, do you have a complete sample program related to ENET module and TCPIP protocol that you can refer to?Thanks for you

0 Kudos
Reply

2,149 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi:

The txrx_transfer is based on enet module, please refer to txrx_transfer example , I take K66f as an example.

SDK_2.6.0_FRDM-K66F\boards\frdmk66f\driver_examples\enet\txrx_transfer

Regards

Daniel

0 Kudos
Reply

2,149 Views
李月鑫
Contributor I

Hi,

If possible, please send me the link of the routine, thank you.

Best Regards

Arlene

0 Kudos
Reply

2,148 Views
danielchen
NXP TechSupport
NXP TechSupport

Please see the attached enet demo for reference.

The whole SDK can be downloaded from below link

Welcome | MCUXpresso SDK Builder 

0 Kudos
Reply