FRDM-K64f ADC and DAC Configuration in MQX RTOS based on KDS 3.0 and KDSK 1.2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-K64f ADC and DAC Configuration in MQX RTOS based on KDS 3.0 and KDSK 1.2.0

1,264 Views
homarpizar
Contributor I

Hi all,

I want to create a project using the ADC in order to read a signal created by the DAC in the same board (FRDM-K64F), but I can´t find any example whit the configuration of these to start the project.

I hope someone can help.

Best regards.

Omar.

Labels (1)
0 Kudos
Reply
1 Reply

857 Views
DavidS
NXP Employee
NXP Employee

Hi Homar,

Please review the baremetal DAC ADC demo.  It could be implemented in a MQX application.

C:\Freescale\KSDK_1.2.0\examples\frdmk64f\demo_apps\dac_adc_demo

Documentation is in: C:\Freescale\KSDK_1.2.0\doc\Kinetis SDK v.1.2.0 Demo Applications User's Guide.pdf Chapter 7.

Regards,

David

0 Kudos
Reply