Case sensitivity of file names

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Case sensitivity of file names

1,156件の閲覧回数
thomasblank
Contributor II

I am using the Freedom Development Board for the KW41z on Linux and have installed KDS and the KW41 Connectivity Software for Linux as outlined in Step 2 of the Getting Started tour at FRDM-KW41Z|Freedom Development Kit|NXP . However, after that I can not follow any of the examples, because in each one I tried I get a lot of compilation errors because both in the file references in the Project Settings and in #include statements, case sensitivity of file names is not taken care of.

 

E.g. I have imported the project at MKW41Z_ConnSw_1.0.2/boards/frdmkw41z/wireless_examples/thread/router_eligible_device_ota_client/freertos/kds, I get numerous errors when I try to build, like

"../../../../../../../../rtos/freertos_8.2.3/Source/include/FreeRTOS.h:98:28: fatal error: FreeRTOSConfig.h: No such file or directory" - A file that I *do* have is "MKW41Z_ConnSw_1.0.2/middleware/wireless/framework_5.3.2/common/rtos/freertos/config/freertosconfig.h"  - in all lower case letters. When I rename that file to the mixed case name, that error goes away, leaving me with only 79 to go.

 

The same problem arises in the generated .project file with the project settings for the IDE. On Project Properties > Resource > Linked Resources > Linked Resources, I get ~40-50 entries with an invalid location. Examplary investigations lead to the problem being that in .project, the referenced file is given as "<locationURI>PARENT-7-PROJECT_LOC/middleware/wireless/ieee_802_15_4_5.3.2/PHY/Source/MKW41Z/Phy.h</locationURI>" I can find the file that I think is meant by this at "MKW41Z_ConnSw_1.0.2/middleware/wireless/ieee_802_15_4_5.3.2/phy/source/MKW41Z/Phy.h" - With a different capitalization at both the names of the folders "phy" and "source".

 

Please advise on how to resolve this problem.

ラベル(1)
2 返答(返信)

978件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Thomas


Please check the post:

https://community.nxp.com/message/866086 


There is a problem with the paths in linux environment.

Hope this information helps you
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

978件の閲覧回数
thomasblank
Contributor II

Hi, Jorge,

I'm sorry, but that is not a good answer. Others and me have that problem, and as I said, there are sometimes hundreds of errors in just one software example. I can not fix all of these by hand and one by one.

What I really wanted to ask is: Is NXP going to fix the SDK on Linux, so that Linux users can evaluate the Kinetis Software Stack?

Cheers,

Thomas