Best approach to transition from a FRDM-K64F board to a custom board?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Best approach to transition from a FRDM-K64F board to a custom board?

跳至解决方案
1,663 次查看
peterfurey
Contributor IV

Hi,

I'm currently developing a prototype application on a FRDM-K64F board that I'll need to port to a custom board using the MK24FN1M0VLL12 processor. I'm using Kinetis Design Studio (Version 3.0.0) and KSDK (Version 1.2.0). My project uses MQX RTOS and PE for Kinetis. Our initial approach to migrate to custom hardware is to stack add-on modules (boards) on top of the FRDM-K64F board and get the components/drivers working for it. For example, the first add-on board is a power board with a user comport and an interface for an altimeter. My question is, when I create the base Kinetis Project using the Processor Expert which derivative makes more sense for a starting point, using the board or the processor (FRDM-K64F or MK64FN1M0xxx12)? Obviously, after we get all the components working and create the final custom board, I'll transition to the MK24FN1M0xxx12 derivative. Does it matter? Or does one make more sense than the other for a starting point?

Much thanks for any opinions,

Peter

标签 (1)
0 项奖励
回复
1 解答
1,388 次查看
peterfurey
Contributor IV

Hi Kan,

Thank you for your reply, the porting guide looks handy. However, it doesn't really answer my question.

I suspect that using the board instead of the processor as a starting point probably makes more sense.

Thanks again,

Peter

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,388 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Peter,

The KSDK 1.2 PEx components also support MK24FN1M0xxx12 devices, you may replace the K64 processor with the one for your custom board. Please also refer to the  attached MQX porting guide for more details. The chapter 5 Changing MCU derivative in MQX projects should be helpful for such kind of porting.

pastedImage_0.png

Hope that helps,


Have a great day,
Kan

Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,389 次查看
peterfurey
Contributor IV

Hi Kan,

Thank you for your reply, the porting guide looks handy. However, it doesn't really answer my question.

I suspect that using the board instead of the processor as a starting point probably makes more sense.

Thanks again,

Peter

0 项奖励
回复