A question in MQX Standard PE component

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

A question in MQX Standard PE component

1,600 次查看
matherinewang
Contributor III

Hi All,

 

i create a new a Kinetis project using Kinetis SDK1.2 and Processor Expert,  and then i add OS componet, and set OS as MQX Standard.

36712_36712.pngpastedImage_6.png      36714_36714.pngpastedImage_9.png

 

After i set as MQX Standard,  PE will add DbgCs1:fsl_debug_console components automatically into Referenced components file foler, shows below.

36708_36708.pngpastedImage_1.png

Then, i got the isue, it's not allowed.  it was added automatically, but then it says not allowed, how can i fix it?

标签 (1)
0 项奖励
回复
4 回复数

1,447 次查看
rqbh
Contributor III

just remove the debug_console component, for mqx has it's own debug out put

0 项奖励
回复

1,447 次查看
matherinewang
Contributor III

Thanks kevin, remove the debug_console componet can fix the problem, but just want to make sure it's okay to remove it.

0 项奖励
回复

1,446 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello Kevin,

yes-exactly. It could be the problem.

Best Regards,

Iva

0 项奖励
回复

1,446 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello matherine wang,

please, can you upload last pic in bigger size?

It is hard to recognize.

Thank you,

Best Regards,

Iva

0 项奖励
回复