请问板子KL27Z的PORT和PIN是怎么确定的?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

请问板子KL27Z的PORT和PIN是怎么确定的?

Jump to solution
778 Views
yanandren
Contributor II

HI,各位技术人员,

你们好

我想请问一下,

1. 根据DATASHEET来看,一共有留个GPIO 的PORT,我想了解一下,根据下面这张图,如何确定这些脚是哪个PORT,哪个PIN,比如左下角,请问是GPIO PORTA  --- pin5,还是别的?

2. 根据评估板来看,是不是能用的脚一共就只有引出来的这些。

 

承蒙关照!

谢谢。

BR

Bernerd

 

 

153591_153591.pngQQ截图20160614134839.png

Labels (1)
0 Kudos
1 Solution
643 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Bernerd,

1.图中对引脚的说明已经指明了对应的port和pin index了,比如说PTB0就是指GPIO PORT B的pin 0。

2.Freedom开发板的扩展接口与Arduino UNO R3版的扩展接口完全兼容,这样就可以和大量的Arduino的扩展板配合使用了。如果你需要检测其他的信号线,就需要根据原理图看能不能飞线出来。

Hi


Wish it helps.

Have a great day,
Kan Li
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
644 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Bernerd,

1.图中对引脚的说明已经指明了对应的port和pin index了,比如说PTB0就是指GPIO PORT B的pin 0。

2.Freedom开发板的扩展接口与Arduino UNO R3版的扩展接口完全兼容,这样就可以和大量的Arduino的扩展板配合使用了。如果你需要检测其他的信号线,就需要根据原理图看能不能飞线出来。

Hi


Wish it helps.

Have a great day,
Kan Li
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos