下载程序时出现Device is permanently secure

キャンセル
次の結果を表示 
次の代わりに検索 
もしかして: 

下载程序时出现Device is permanently secure

258件の閲覧回数
yanandren
Contributor II

HI,ALL

 

我在使用keil给我的MKL27Z64VLH4下载程序的时候出现了如下的提示,请问有什么办法可以解除板子的secure.

 

 

谢谢。

 


152779_152779.pngQQ图片20160603124736.png

 

 

152885_152885.pngQQ图片20160603124750.png

ラベル(1)
0 件の賞賛
2 返答(返信)

140件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi YAN.

Thank you for your feedback.

Just click on yes, it should works without problems now.

QQ图片20160603124736.png

Please, let me know if it works you.

Best Regards,

Iva

0 件の賞賛

140件の閲覧回数
yanandren
Contributor II

Hi Iva,

Thanks for the answer.

But the 'Comfirm' dialog showed up twice and then jump to the 'PEMICRO connection manage' dialog.

Only clicked YES can't solve my issue.

Is there any possibility that the Board had been locked ?

BR

Bernerd

0 件の賞賛