使用KL27ZM64配置GPIO输入输出的时候有一个上拉

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

使用KL27ZM64配置GPIO输入输出的时候有一个上拉

736 Views
yanandren
Contributor II

请问一下,

我在配置KL27ZM64的GPIO口输入或者输出的时候有一个上拉,配置完以后就是默认高电平,请问如何可以不用这个上拉。

 

承蒙关照。

Labels (1)
0 Kudos
2 Replies

626 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Bernerd,

请问使用了哪个版本的ksdk?可以贴一段初始化代码上来看看吗?谢谢!

Have a great day,
Kan Li
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

626 Views
yanandren
Contributor II

SDK版本:SDK_2.0_FRDM-KL27Z

#define IO_GPIO  GPIOB                                               //定义SDA的GPIO

#define IO_PIN   0   

#define IO_OUT    IO_GPIO->PDDR |= (1U << IO_PIN);             //配置输出      

#define IO_IN        IO_GPIO->PDDR &= ~(1U << IO_PIN);            //配置输入

static inline void Slave_Send_Byte(uint8_t snd)

{

  uint8_t loop=0;

  IO_OUT();

  //此处是函数体,就是给IO发送一些bit,发送完以后配置成输入模式

 

  IO_IN();

}

0 Kudos