nano-edge at Kinetis E Series

cancel
Showing results for 
Search instead for 
Did you mean: 

nano-edge at Kinetis E Series

284 Views
amerzater
Contributor III

Hello 

dose the Kinetis E Seris support nano-edge for High Resolution PWM.

I need a 5V robust MCU with High resolution 50KHz PWM .

could you please suggest a solution

Labels (1)
0 Kudos
1 Reply

264 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Amer,

No, none of KE series device has nano-edge pwm. But if high FlexTimer working clock can improve PWM performance, you can use KE1xZ and KE1zF. KE1xZ FlexTimer max clock frequency is 72Mhz, and KE1xF is 168Mhz.

If that is not enough, you can only select KV4x and KV5x. They are 3.3v device.

Regards,

Jing

0 Kudos