kms与twr-kv31f120板连不上

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

kms与twr-kv31f120板连不上

跳至解决方案
2,927 次查看
wendychen
Contributor I

我有一个由TWR-KV31F120M板、TWR-MC-LV3PH板和45ZWN24-40电机组成的评估系统,可以运行MCRSP-PMSM-V1.1.1参考解决方案。但这个系统与KMS(kinetis motor suite)总也连不上,每次总是提示“Could not verify communication over port COMxx”,不知是什么原因。我的TWR-KV31F板是今年3月才买的,我也在WIN8和WIN10上都试了,结果都一样

标签 (1)
0 项奖励
1 解答
2,416 次查看
philip_drake
NXP Employee
NXP Employee

The low cost reference platform to get you started with KMS is available to order from nxp.com(here).  You will need the following

  1. FRDM-KV31Fsmall_frdm_kv31.png
  2. FRDM-MC-LVPMSM small_frdm_pmsm.png
  3. FRDM-MC-LVMRTsmall_linuxmotor.png

You may provide your own PMSM motor for the testing. TheLVPMSM shield is typically used for up to 24V 5.1 Amp motors only.

Philip

在原帖中查看解决方案

0 项奖励
3 回复数
2,416 次查看
philip_drake
NXP Employee
NXP Employee

I am assuming this tower board has been enabled for KMS at the factory. If not you will need to order a new TWR-KV31F512 board for use with Kinetis Motor Suite.  The debugger must be "MSD-DEBUG-TWR-KV31F12_Pemicro_v118.SDA" or later.

If it is a KMS enabled TWR board and the debugger version is correct, then please try starting from a new KMS project, once KMS tries to open the serial port it might ask you to load the new project onto the MCU.  If it does not use the project --> load .out file function to load the KMS project onto the TWR board.  After this has completed and if there is voltage supplied to the LV3PH then the yellow LED  will flash slowly on the TWR board.  If there is a RED LED you may have a fault condition due to jumper issues. consult the KMS users guide for jumper placement.

Once the yellow light is flashing try communicating with the TWR board.

0 项奖励
2,416 次查看
wendychen
Contributor I

我的TWR-KV31F120板上的ARM确实不是那种支持KMS特性的版本,芯片型号不带字母P尾缀。我想再买一套FRDM系列的评估板,不知网上从哪里能买到肯定具有KMS特性的版本。

Sent from Windows Mail

0 项奖励
2,417 次查看
philip_drake
NXP Employee
NXP Employee

The low cost reference platform to get you started with KMS is available to order from nxp.com(here).  You will need the following

  1. FRDM-KV31Fsmall_frdm_kv31.png
  2. FRDM-MC-LVPMSM small_frdm_pmsm.png
  3. FRDM-MC-LVMRTsmall_linuxmotor.png

You may provide your own PMSM motor for the testing. TheLVPMSM shield is typically used for up to 24V 5.1 Amp motors only.

Philip

0 项奖励