KV31F with KMS Not Working!!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KV31F with KMS Not Working!!

3,587 Views
trialaccount12
Contributor V

Hi,

     I am trying to use KMS 1.1.0 with KV31F.

Initially, I flashed KV31F with KDS 3.2.0 demo program (PMSM_ref_sol). It worked. I was able to control the motor speed using freemaster and SW2. 

But when I try to use KMS with KV31F, it says it could not verify the communication over the UART port. 

(The same UART port worked perfectly for KDS program).

Can anyone tell me what's the problem?

I went through the community and it mentioned the KMS image not being flashed properly onto the KV31F board.

How do I check it?

I tried all the troubleshooting. Putting into bootloader and open SDA again. But it still does not work. Two boards, I have the same error. 

Thanks and Regards

Niranjan

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

3,484 Views
philip_drake
NXP Employee
NXP Employee

Please see the announcement about KMS. https://community.nxp.com/community/general-purpose-mcus/kinetis/kms 

Regards,

Philip

0 Kudos
Reply