Drag and Drop programming will work with a .srec or .bin type file. file the .axf file, right mouse click and choose the binary tool and create a .bin. You can drag and drop these files.
- NXP no longer licenses the 3rd party IP that was part of our KMS offering.
- Our ability to support customers on that platform is severely compromised
- We recommend all customers to transition onto NXP owned enablement/IP.
You will be able to run your motor but not with the KMS tools and software.
With the boards you have you can still drive your motor fairly easily.
You can start by use MCUXpresso IDE , the KVxx SDK and the motor control middle-ware. The demo will get you started with motor control.
The next step is to get the PMSM reference design software from here and the FreeMaster tool here These installations still rely on the Kinetis Design Studio IDE. These are being ported to the latest IDE MCUXpresso later this year.
- 3-Phase Permanent Magnet Synchronous Motor (PMSM) Control Reference Design
- The 3-Phase Permanent Magnet Synchronous (PMSM) Motor Control Reference Design is based on Kinetis® V Series MCUs and intended to provide the example for 3-phase sensorless PMSM motor control solutions. The Reference design utilizes closed-loop field oriented vector speed (FOC) control mechanism.
Regards,
Philip