Hi gobi s
This error occurs when you are no selecting you interface correctly, Could you explain you case more:
Debug configuration?
What example code are you using?
MCU that you are using?
Regards
Jorge Alcala
Hi Jorge,
Thanks for your reply...sorry for late reply,,
Details below about your questions..
Debug configuration?
GDB PEMicro Interface debugging
MCU that you are using?
Our freescale controller is MKE02Z64 VQH4(MODEL: FDRM-KE02740M)..into
controller MKE02Z16VLC4 I want to flash.
What example code are you using?
Actually i am using the code which already developed by some one...no
error in that because who developed that code they had flashed &
checked..in my end it is not happening...i need your support to finish
that flashing..
Thanks
S.Gobi
Hi gobi s
Could you share a screenshot of your debug configuration? in P&E micro it should appear selected an Interface and a PORT in the debug configuration window as follow in the next image:
If you are not able to select both of them, please check that your device manager can identify your debug interface and let me know what you get.
Hope this helps,
Best Regards
Jorge Alcala
Hello,
a common reason for that "error in services launch sequence" message is that there is a dangling GDB server. See https://mcuoneclipse.com/2015/05/18/gdb-client-and-server-unlocking-gdb/ . Can you check that the P&E GDB server is not still running (if so, kill it in the task manager)?
I hope this helps,
Erich
Hi jorge,
plz find the attachment of screenshot of my debug configuration..as you said
port i cant able to select but in device manager, i checked driver for
freescale got installed . Eventhough i cant select port..
Thank you
Jorge Antonio Alcala Vazquez
replied to the discussion
"Re: while flashing i got this error "{Error in services launch sequence}"
plz give sollution to solve this"
To view the discussion, visit:
https://community.nxp.com/message/839432?commentID=839432&et=watches.email.thread#comment-839432
>