Hi antonio,
Thank you for the interest in NXP kinetis product, I would like to provide service for you.
Now, answer you several questions:
1. Why the standard driver is not included?
Answer: Actually, dspi is the SPI which you need, just in the K28 MCU, the SPI module name is DSPI.
Don't worry, you can use that dspi examples.
2. Can I use the device as a simple SPI master using any of this driver?
- After googling I read that is possible, so:
2a. What is the correct configuration? What should I watch out for?
2b. There is an example of this use case?
Answer: Please refer to the official SDK code for K28, which can be downloaded from this link:
Welcome | MCUXpresso SDK Builder
Please choose the chip as MK28, then generate the code and download it.
After you download the code, you can find the dspi sample code in folder:
\FRDM-K28F\boards\frdmk28f\driver_examples\dspi
Please try it on your side, each example have the readme.txt help you to understand it.
If you still have question about it, please kindly let me know.
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------