using 6 uarts and 2 spi ans 2 IIC along with USB and ethernet simultaneously

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

using 6 uarts and 2 spi ans 2 IIC along with USB and ethernet simultaneously

892 Views
kumark
Contributor I

I want to use 6 uarts and 2 spi ans 2 IIC along with USB and ethernet. But in the pin multiplexing I cant find all these options together even if I take a MCU with all these features. Am I getting wrong somewhere or is it not possible to use all these together.

0 Kudos
Reply
1 Reply

781 Views
miduo
NXP Employee
NXP Employee

Yes, your concern is correct. Even for the Kinetis parts who has all the interface you mentioned, but they can not been enabled simultaneous. For example, the UARTs are multiplexed with SPIs. So you can only use one function at a time.

0 Kudos
Reply