unable to install the kinetis 100Mhz tool kit for windows

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

unable to install the kinetis 100Mhz tool kit for windows

ソリューションへジャンプ
1,495件の閲覧回数
vallinaths
Contributor II

hi

  purchased the TWR-K60D100M development and download the com.freescale.mcu10_2.Kinetis_100MHz_K10_K20_K30_K40_K50_K60.win.v1_0_2 from the freescale website and unzip the file and trying to run the content.jar executable file .and getting an error "invalid or corrupted jar file " having Jdk 6 and jre7 version java . Please let me know the solution to problem

thanks

vallinath

ラベル(1)
0 件の賞賛
返信
1 解決策
1,324件の閲覧回数
apanecatl
Senior Contributor II

The "toolkit" you make reference to is a CodeWarrior 10.2 update, it is not an executable file, you need to install it from the CodeWarrior menu in the following manner:

1 Open CodeWarrior 10.2

2 On the upper tool menu click on help > install software

3 Click on the add button to the right of the work with address bar

4 A new window will pop up, click on the archive button and navigate to the root folder where you saved the update file and   click ok

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,324件の閲覧回数
vallinaths
Contributor II

thanks works fine

0 件の賞賛
返信
1,324件の閲覧回数
Monica
Senior Contributor III

Vallinath, were this suggestions useful?

We'd like to know!

Regards!

0 件の賞賛
返信
1,325件の閲覧回数
apanecatl
Senior Contributor II

The "toolkit" you make reference to is a CodeWarrior 10.2 update, it is not an executable file, you need to install it from the CodeWarrior menu in the following manner:

1 Open CodeWarrior 10.2

2 On the upper tool menu click on help > install software

3 Click on the add button to the right of the work with address bar

4 A new window will pop up, click on the archive button and navigate to the root folder where you saved the update file and   click ok

0 件の賞賛
返信