twr-k70--> Failed to Open. Plug DEMO board into PC via USB cable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

twr-k70--> Failed to Open. Plug DEMO board into PC via USB cable

950 Views
francescogerard
Contributor I

when i try to connect the twr k70 with the terminal utlity i can not open the port and i read  "Failed to Open. Plug DEMO board into PC via USB cable" even if with another program that putty i open the com.

another problem is that the osbdm is not recognized as a usb com but as a generic com.

i try to follow the troubleshooting guide from pemicro site but nothing...

can anyone help me?

Tags (1)
0 Kudos
Reply
5 Replies

693 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

"t the osbdm is not recognized" , so does your project have been download to the board?

Please check the J10 on board, do not connect the pin 1 and 2 of J10.

Then the normal situation is like this :

pastedImage_0.png

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

693 Views
francescogerard
Contributor I

Hi

Osbdm is normally recgonized buti f i check in computer i dont see the peripheral. Is normal?

If I create an exe how to load this file in the tower?

thanks

Da: Alice_Yang

Inviato: lunedì, 7. marzo 2016 10:43

A: Francesco Gerardi <gerardi@orchestraweb.com>

Oggetto: Re: - twr-k70--&gt; Failed to Open. Plug DEMO board into PC via USB cable

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community

twr-k70--> Failed to Open. Plug DEMO board into PC via USB cable

reply from Alice_Yang <https://community.freescale.com/people/Alice_Yang?et=watches.email.thread> in Kinetis Microcontrollers - View the full discussion <https://community.freescale.com/message/622012?et=watches.email.thread#comment-622012>

0 Kudos
Reply

693 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Francesco,

- Although you can not find it in the computer management , how do you know

"Osbdm is normally recgonized" ?

- About how to download the project to board , please refer to the screenshot :

pastedImage_0.png

if the board is recognized , it will show in the Port :

pastedImage_1.png

then click "Debug", if it show update the firmware, please refer to the reminder to operate ,

in teh TWR-K70 board , the bootloader header is J10:

pastedImage_2.png

click OK, when it start update ,you can see

pastedImage_3.png

After the update , you can download it now .

If still have problem on your side ,please also take a screenshot about it , then we can solve

it sooner .

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

693 Views
francescogerard
Contributor I

Hi

I have another question for you :smileyhappy:

I have download egui demo and I would upload this in the twr-k70 .

Which program I have need to do this? I can upload this only with the usb ?

thanks

Da: Alice_Yang

Inviato: mercoledì, 16. marzo 2016 09:52

A: Francesco Gerardi <gerardi@orchestraweb.com>

Oggetto: Re: - twr-k70--&gt; Failed to Open. Plug DEMO board into PC via USB cable

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community

twr-k70--> Failed to Open. Plug DEMO board into PC via USB cable

reply from Alice_Yang <https://community.freescale.com/people/Alice_Yang?et=watches.email.thread> in Kinetis Microcontrollers - View the full discussion <https://community.freescale.com/message/625304?et=watches.email.thread#comment-625304>

0 Kudos
Reply

693 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

HI,

You can also use some other debuggers , for example P&E multilink .

Alice

0 Kudos
Reply