suggestion on Flash programming for Production on K60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

suggestion on Flash programming for Production on K60

1,068件の閲覧回数
vallinaths
Contributor II

Please suggest exact method and best methodology which can used for flash programming of K60 chip .

the board has following interfaces : Ethernet , RS232,RS485

IDE; IAR WORKBENCH

controller : 100 pin

Debugger : OLIMEX-ARM-USB-OCD

the application we have as the ethernet & serial interfaces and we need to plan for the production . the image file to be used and excat method to be followed .

can we use ethernet boot loader or openocd can be used as standalone flash programmer .

thanks & regrds

vallinath

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

850件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello vallinath:

We are sorry that you did not receive a response.

Did you clarify your doubt?

I cannot comment about the OLIMEX-ARM-USB-OCD tool, but since Kinetis parts are based on ARM cores, the available tools and programming solutions are many. It just depends on your needs.

Regarding bootloaders:

Ethernet: http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4367.pdf

Serial: http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295.pdf

Regards!

Jorge Gonzalez

0 件の賞賛
返信

850件の閲覧回数
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. Kinetis Microcontrollers ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.

0 件の賞賛
返信