"Permission Denied" When Installing Supplied VCOM Driver on Windows 7

キャンセル
次の結果を表示 
次の代わりに検索 
もしかして: 

"Permission Denied" When Installing Supplied VCOM Driver on Windows 7

ソリューションへジャンプ
419件の閲覧回数
razed11
Contributor V

I downloaded SDK 2.4.2 for the K64 (USB & FreeRTOS) and built `usb_device_cdc_vcom`. When plugged in to a Windows 7 Professional machine I see `MCU VIRTUAL COM DEMO` in the device manager. When I follow the steps in the README PDF I get:

Windows found driver software for your device but encountered an error while attempting to install it.

Virtual Com Port

Access is denied.

I've checked permissions (owned by me and I'm an administrator). If I double click `cdc.cat` it claims that it is valid. I thought it might be related to digital signing but I'm not getting error to that effect.

Hoping to use this for a production device and it'd be nice to not use an FTDI chip + UART.

Thanks.

ラベル(2)
0 件の賞賛
1 解決策
303件の閲覧回数
razed11
Contributor V

User error: I had copied the .inf file from my Mac and the line endings were incorrect. Used unix2dos to convert the line endings and all is well.

元の投稿で解決策を見る

0 件の賞賛
1 返信
304件の閲覧回数
razed11
Contributor V

User error: I had copied the .inf file from my Mac and the line endings were incorrect. Used unix2dos to convert the line endings and all is well.

0 件の賞賛