"Multiple markers at this line" in Codewarrior during debug of Kinetis L on FRDM board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

"Multiple markers at this line" in Codewarrior during debug of Kinetis L on FRDM board

跳至解决方案
5,270 次查看
steve_fae
Senior Contributor I

Somehow now, no matter where I try to put even a single break statement, I get the error "Multiple markers at this line" so the break point marker which should be a dot becomes a dot with a cross through it.  I have tried to place a break statement at the C source line or even the assembly source line and I get the same error.  Any idea what is messed up?

标签 (1)
1 解答
3,112 次查看
BlackNight
NXP Employee
NXP Employee

I have found what could make the breakpoint icon to have this line:

3146_3146.png

在原帖中查看解决方案

6 回复数
3,112 次查看
BlackNight
NXP Employee
NXP Employee

Could you check what you have listed in the 'Breakpoints' view? Looks like you have multiple breakpoint types set on a single line?

0 项奖励
回复
3,112 次查看
steve_fae
Senior Contributor I

So I cleared all breakpoints first.  Then added one at a line of C.  Still get the breakpoint with a line through it.  In breakpoint view see processor expert checked of regular type and below it and then one in main in the project.elf file at a virtual address of regular type.

0 项奖励
回复
3,113 次查看
BlackNight
NXP Employee
NXP Employee

I have found what could make the breakpoint icon to have this line:

3146_3146.png

3,112 次查看
dalelee
Contributor II

Yes i had the same issue. It was the exact same problem.

Thanks for the posting.

0 项奖励
回复
3,112 次查看
steve_fae
Senior Contributor I

Very weird.  I played with the settings of breakpoint view but nothing was improving. When I changed the view from breakpoints to variable view, now breakpoints work.  No clue..

0 项奖励
回复
3,112 次查看
BlackNight
NXP Employee
NXP Employee

Yes, weird. I do not remember that I have seen such a breakpoint icon with that line.

0 项奖励
回复