problem with kinetis_sc lcdc example on twr-k70f120m

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem with kinetis_sc lcdc example on twr-k70f120m

ソリューションへジャンプ
4,224件の閲覧回数
claudiomechini
Contributor II

Good morning, My name is Claudio Mechini and I am a software developer of the LED SpA company. We have to evaluate the LCDC controller features of the kinetis K70 so we have bought the tower system TWR-K70F120M with TWR-SER module and TWR-LCD-RGB module. With this configuration I had flashed the micrcocontroller with your LCDC demo example (and also lcdc_rev2) of the package "KINETIS SC" but I have a problem. When the demo start the display of the twr-lcd-rgb show for just a second the correct windows composed by four square of different color,red,green,blue and white and a center rectangle with black colour (IM008804.jpg), and then show other windows with rows and columns of random colours like the clock is absent(IM008805.jpg and IM008806.jpg) , but all the signals, hsync,vsync,clk,de, are present, I have controlled them with digital scope. So what is the cause? I have tried also with lcdc-rev2 demo but there is the same issue. I hope that you can help me. Thanks you. Best regards

ラベル(1)
0 件の賞賛
返信
1 解決策
3,950件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello Claudio,

Please try to change the lcdc.c file in your project for the attached. That configuration is working in all the TWR-LCD-RGB revisions.

Best Regards,

Luis

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,951件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello Claudio,

Please try to change the lcdc.c file in your project for the attached. That configuration is working in all the TWR-LCD-RGB revisions.

Best Regards,

Luis

0 件の賞賛
返信
3,950件の閲覧回数
claudiomechini
Contributor II

Thank you very very much Luis. Now can I go to the next step. Have a nice day. Best regards. Claudio

0 件の賞賛
返信