ping_demo

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ping_demo

909 次查看
maheshwarreddy
Contributor I

hi,

iam using the ping demo application in k66 from sdk2.0 but i can able to send the data which is available at output of the processor but iam not able to see the data in wireshark. if i make the phy loopback the tx data and enable signals are same, what is the problem iam not getting can help us.

0 项奖励
回复
1 回复

799 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

I also do a  test with FRDM-K66F board and lwip_ping_bm demo, with below test result:

pastedImage_1.png

The FRDM-K66F board could get response from PC( IP address: 192.168.1.100).


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复