Hi, I'm working gstreamer using imx8mqevk.
My goal is rtp streaming.
But, I have a camera not detected problem.
Please refer to below the capture.
I confirmed that the camera works well in kernel version 4.9.88 and yocto version is imx-linux-rocko.
To achieve my goal, I upgrade yocto version and add PACKAGECONFIG_mx8mq = "x264" in local.conf.
(Because imx8m don`t have H/W encoder. I want use S/W encoder.)
My kernel version is 4.14.98 and yocto version is imx-linux-sumo(manifest is "imx-4.14.98-2.0.0_ga.xml")
Yours solution is my pleasure!!!!!
Thank you!!!
what dts file do you use?did you use the dts file with camera?