need help using irda on k60n512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

need help using irda on k60n512

Jump to solution
1,192 Views
wolfbang
Contributor I


hi,

i am a student and for a mini project i was given the assignment of communicating between a computer, using usb to irda converter on my laptop, to the tower k60 using irda. As the k60 is new to me and i ve never used irda before i was hoping if i outlined how i configured the board someone would be kind enough to outline any configuration or concept errors i may be making as i cant seem to get the controller to work.

1. I am sending out a character from a serial monitoring program through the usb which is converting the signal to irda through the converter.

     The idea for the moment is to recieve the character, through the irda, to UART0, and just echo it to the P&E terminal. But having no joy

2. I have the comparator set in continuous conversion mode.CMP0 enabled and CMP0 = COUTA. Using the DAC as the ref voltage, 1v,and selecting IN0       as PMUX input and IN7 as MMUX input.

3. I have CMP0 as uart input and PORTC_PC6 as alternative 1 for CMP0

Using baud rate of 115.2k. If i have made any errors in my configurations i would really appreciate the help.Thanks very much

Labels (1)
0 Kudos
Reply
1 Solution
856 Views
DavidS
NXP Employee
NXP Employee

Hi Wolfbang,

The Freescale KwikStik (Kinetis K40 with Segment LCD and lots of peripheral support on and off chip) has IrDA support.

Please visit the web page for documentation and downloads.

Regards,

David

View solution in original post

0 Kudos
Reply
1 Reply
857 Views
DavidS
NXP Employee
NXP Employee

Hi Wolfbang,

The Freescale KwikStik (Kinetis K40 with Segment LCD and lots of peripheral support on and off chip) has IrDA support.

Please visit the web page for documentation and downloads.

Regards,

David

0 Kudos
Reply