mingw32-make: *** [HORNO2.elf] Error1 help me!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mingw32-make: *** [HORNO2.elf] Error1 help me!

2,572 次查看
alejandro_df
Contributor I

I have an application where I am using kl25. with usb stack with  processor expert does not send a single error in the code but when copilar just sends me the following error:
Description Resource Path Location Type
mingw32-make: *** [HORNO2.elf] Error 1 HORNO2 C / C + + Problem



Message was edited by: Monica Arvizu

0 项奖励
回复
3 回复数

1,388 次查看
apanecatl
Senior Contributor II

I suggest you include your project code to review it, the mingw32-make error is quite common and not very specific, also include the part you are using, i.e.: MK60DN512

0 项奖励
回复

1,388 次查看
alejandro_df
Contributor I

Sorry. the warnings are from another project. my project does not send a single warning

0 项奖励
回复

1,388 次查看
Monica
Senior Contributor III

Hola Alejandro!

I removed the warning section from your post to avoid confusion...let me know if any concern.

Best regards,

Monica.

0 项奖励
回复