measured voltage on a pin connected to ground by 4M7 resistor.....kl14 ADC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

measured voltage on a pin connected to ground by 4M7 resistor.....kl14 ADC

1,417件の閲覧回数
stefanomanca
Contributor III

Hi, I have an ADC pin connected to ground by a 4.7Mohm resistor. When I read the value by adc I get 32 that means 32*(2.5V/255)=310mV if the reference voltage is 2.5Volt and the resolution is 8 bit.

I wander why the value is so big, it should by almost zero.

Any idea.

How can reduce the sampled value.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,258件の閲覧回数
mjbcswitzerland
Specialist V

Hi

pastedImage_0.png

pastedImage_2.png

0...1uA x 4.7M = 0...4.7V. In your case Iin must be about 66nA. From the data sheet it could be a lot more and you will probably find that if you heat the device the error will increase a lot.

To ensure accuracy you need to have a low impedance input source; 4.7M is much too large for any accuracy to be ensured. Eg. Add a voltage follower between the input source and the ADC.

Regards

Mark