kw41z reset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

kw41z reset

1,368 次查看
sheshnathchauha
Contributor II

Hi,

i have use kw41z controller for my ble project but my board is not programming because when i powered my board its always be  in reset  .so kindly give me suggestion ,here i am attching my reset circuit please go through .

thank you

kind

regard

sheshnathRESET.png

2 回复数

1,134 次查看
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Sheshnath,

Can you check the reset signal on an oscilloscope? On blank chips, the expected behavior is a saw wave because the MCU keeps resetting as it is loading an invalid address to the stack pointer and program counter. Once flashed, the reset should stop oscillating. 

For the SWD connections refer to the section 2.1.5.1 Debug interface of the document KLQRUG.

Regards,

Gerardo

0 项奖励
回复

1,134 次查看
diegocomin
Contributor IV

Hi Gerardo,

I have posted my issue confirming the saw wave which I obtain in my blank module (Reset error, debugging KW41Z with an external J-link Base tool), but when I try to flash it (debug) with a J-link tool I always obtain this error:  "Connect under reset", "Communication error while accessing MDM-AP" and the J-Link LED turn red (because it is always resseting).

How can I solve this problem? Please I really need a solution.

 

Diego C.