kinetis SDK_S32K1xx_13 is not installed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kinetis SDK_S32K1xx_13 is not installed

Jump to solution
2,118 Views
liuxing_hu
Contributor III

when I open a s32ds project based on FS32k116 , the error happened, it indicates that I need to install kinetis SDK_S32K1xx_13, but I can't found where can I find installation and how to install

s32ds version:   2.2

0 Kudos
Reply
1 Solution
2,111 Views
nxf58904
NXP Employee
NXP Employee

Hi,

The step as follows,

nxf58904_1-1606986460850.png

nxf58904_3-1606986538903.pngnxf58904_4-1606986555236.png

 Jianyu: 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

View solution in original post

0 Kudos
Reply
1 Reply
2,112 Views
nxf58904
NXP Employee
NXP Employee

Hi,

The step as follows,

nxf58904_1-1606986460850.png

nxf58904_3-1606986538903.pngnxf58904_4-1606986555236.png

 Jianyu: 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 Kudos
Reply