kinetis KL2x programming voltage @ 1.8V

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

kinetis KL2x programming voltage @ 1.8V

跳至解决方案
2,079 次查看
heng
NXP Employee
NXP Employee

Hi

How to program the flash memory @1.8V VDD?

The tools that i have tried are

1) P&E (Green color) USB Multilink

2) P&E FX  (black color) USB mutlilinks

3) J-link lite

All required at least around 2.7V VDD to download the binary into the flash memory of KL26 via SWD protocol.

I have tried on IAR 7.20 and CW10.6 ID and have removed all the active components on the freedom board of KL26 (freedom REV B) but it still does not work.

The debugging and the flash programming only will only work when the VDD is around 2.7V.

Can we program the flash memory of kinetis KL2x @ 1.8V VDD?

From the RM, it show 1.71V to 3.6V with flash programable down to 1.71V with fully functional flash and analog peripherals.

What is the tools we can use to program the flash memory @ 1.8V VDD?

Do we need to adjust a lower value of 10k and 4.7K of the pull-up resistors at reset pin and SWD_DIO pin respectively?

Many thanks.

Best Regards

Heng

标签 (1)
0 项奖励
回复
1 解答
1,691 次查看
heng
NXP Employee
NXP Employee

got it done via CW10.x and P&E USB mulitlink but it cannot be done with OPENSDA

1) KL26 freedom board, FRDM-KL26Z. REV B

remove the resistors of R2, R3, R4

cut the trace line below the jumpers of J13

pump in the power supply of 1.8V @ J5 pin, P3V3_KL26Z

2) KL25 freedom board, FRDM-KL25Z, REV E

Remove the resistor, R74, R81, R73

cut the trace line below the jumpers of J14,

pump in the power supply of 1.8V @ J4 pin, P3V3_KL25Z

Thanks,

Regards

Heng

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,692 次查看
heng
NXP Employee
NXP Employee

got it done via CW10.x and P&E USB mulitlink but it cannot be done with OPENSDA

1) KL26 freedom board, FRDM-KL26Z. REV B

remove the resistors of R2, R3, R4

cut the trace line below the jumpers of J13

pump in the power supply of 1.8V @ J5 pin, P3V3_KL26Z

2) KL25 freedom board, FRDM-KL25Z, REV E

Remove the resistor, R74, R81, R73

cut the trace line below the jumpers of J14,

pump in the power supply of 1.8V @ J4 pin, P3V3_KL25Z

Thanks,

Regards

Heng

0 项奖励
回复