kStatus_UART_NoiseError is set on line with about 340mV of noise

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kStatus_UART_NoiseError is set on line with about 340mV of noise

ソリューションへジャンプ
1,317件の閲覧回数
stdcerr
Contributor IV

Hi,

 

I'm attempting to receive data from UART4 on our custom board but UART_ReadBlocking returns kStatus_UART_NoiseError even though there's minimal error on the actual MCU's Rx pin.

The UART in question is receiving data from a RFID reader at 9600bps while I also have a debug UART setup at 115200 bps. They are both configured with the same clock frequency and hence I think that my clocking should be okay. More particular, I pass "CLOCK_GetCoreSysClkFreq()" as uint32_t srcClock_Hz to UART_Init().

Since the noise on the line doesn't seem to cause havoc either, what else might be causing this issue?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,310件の閲覧回数
stdcerr
Contributor IV

If you get here with the same or a similar problem, check your clock source setup, turns out I didn't initialize the UARTs with the correct clock sources myself. I had to use UART4_CLK_SRC to feed into CLOCK_GetFreq() to get the correct frequency for the different UART modules.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,311件の閲覧回数
stdcerr
Contributor IV

If you get here with the same or a similar problem, check your clock source setup, turns out I didn't initialize the UARTs with the correct clock sources myself. I had to use UART4_CLK_SRC to feed into CLOCK_GetFreq() to get the correct frequency for the different UART modules.

0 件の賞賛
返信