k64f that reboots every 30 seconds, any ideas

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

k64f that reboots every 30 seconds, any ideas

945件の閲覧回数
davidatkins
Contributor I

Got my brand new from farnell FRDM k64F but it reboots every 30 seocnds, a driver appears in wod nows for it then 10 secodns or so later it reboots and disconnects, I think I saw the RGB led light briefly on first boot. not sure if this is a clash with drivers, have uninstalled the driver that was in the device manager, 

Any ideas?

0 件の賞賛
返信
2 返答(返信)

834件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi David,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.

I'd highly recommend that you can program some SDK's demos to the K64, then check the run result to confirm the chip whether work well or not.

You can download the KSDK through the link below.

Software Development Kit for Kinetis MCUs|NXP
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

834件の閲覧回数
davidatkins
Contributor I

Hi,

got that doine with help from someone who had managed to get to the same point, tryign to debug now but cannot get the dbeuggign to work with the bubble demo, openocd is not found and i cannot see an installed for it, gave i missed somehting?

0 件の賞賛
返信