is kinetis k40 internal voltage regulator internally connected to core?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

is kinetis k40 internal voltage regulator internally connected to core?

1,017 Views
pablo_slavkin
Contributor I

Hi, I'm trying to use the internal voltage regulator of the k40, but I don't know if  I'd wire on on the PCB the 3v3out to all VDD of the IC to get the uC run.... or if it's internally connected to the core and peripherals. and let the VDD pins unconnected..

I could't find the block diagram of the internall setup so I'm confusing....

thanks in advance for your time.

Pablo

0 Kudos
Reply
2 Replies

887 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Pablo:

I think you refer to USB regulator, right?

This regulator is not internally connected to the core or peripherals, so yes, you need to wire externally to VDD. Just place a capacitor between Vreg33out and GND (~ 2.2 uF). AND make sure not to exceed the maximum 120 mA.


Regards!
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

887 Views
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. Kinetis Microcontrollers ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.

0 Kudos
Reply