how to Unbrick a frdm-k64f

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to Unbrick a frdm-k64f

1,924 次查看
unclemike
Contributor III

I am trying to unbrick two frdm-k64f boards.  I looked at the info at mcuoneclipse.com and tried the following:

I used CW 10.7 and Processor Expert to make a dummy app for a K20.  All it does is toggle the led that is connected to port D4 fo the K20.  I use a PEMicro multilink to download the app and I can debug, step, etc. just fine. LED works.

Then I use "flash file to target" and download 0244_k20dx_bl_0x5000.bin.  I power cycle the board and there are no LED's lit and no USB MSD appears.  The output from the flash operation is:

***************

fl::target -lc "LC for Simple Flash"
fl::target -b 0x1fffe000 0x4000
fl::target -v off -l off
cmdwin::fl::device -d "FTFL_PFlash128S1RAM16" -o "32Kx32x1" -a 0x0 0x1ffff
cmdwin::fl::image -f "C:\\Users\\micha\\Downloads\\0244_k20dx_bl_0x5000.bin" -t "Auto Detect" -re on -r 0x0 0x1ffff -oe off
cmdwin::fl::erase image
Beginning Operation ...
-------------------------
Auto-detection is successful.
File is of type Binary/Raw Format.

Performing target initialization ...
failed on register write: ETF_FCR
Downloading Flash Device Driver ...
Reading flash ID ...
Erasing Sector 0x00000000 to 0x000003FF
Erasing Sector 0x00000400 to 0x000007FF
Erasing Sector 0x00000800 to 0x00000BFF
Erasing Sector 0x00000C00 to 0x00000FFF
Erasing Sector 0x00001000 to 0x000013FF
Erasing Sector 0x00001400 to 0x000017FF
Erasing Sector 0x00001800 to 0x00001BFF
Erasing Sector 0x00001C00 to 0x00001FFF
Erasing Sector 0x00002000 to 0x000023FF
Erasing Sector 0x00002400 to 0x000027FF
Erasing Sector 0x00002800 to 0x00002BFF
Erasing Sector 0x00002C00 to 0x00002FFF
Erasing Sector 0x00003000 to 0x000033FF
Erasing Sector 0x00003400 to 0x000037FF
Erasing Sector 0x00003800 to 0x00003BFF
Erasing Sector 0x00003C00 to 0x00003FFF
Erasing Sector 0x00004000 to 0x000043FF
Erasing Sector 0x00004400 to 0x000047FF
Erasing Sector 0x00004800 to 0x00004BFF
Erasing Sector 0x00004C00 to 0x00004FFF
Erasing ...
Erase Command Succeeded
cmdwin::fl::write
-------------------------
Using restricted address range 0x00000000 to 0x0001FFFF
Programming file C:\Users\micha\Downloads\0244_k20dx_bl_0x5000.bin
Auto-detection is successful.
File is of type Binary/Raw Format.

Downloading Flash Device Driver ...
Reading flash ID ...
Auto-detection is successful.
File is of type Binary/Raw Format.

Downloading 0x00003310 bytes to be programmed at 0x00000000
Executing program ....
Program Command Succeeded
Downloading 0x00001CF0 bytes to be programmed at 0x00003310
Executing program ....
Program Command Succeeded
cmdwin::fl::device -d "FTFL_DFlash32S1RAM16" -o "8Kx32x1" -a 0x10000000 0x10007fff
cmdwin::fl::image -f "C:\\Users\\micha\\Downloads\\0244_k20dx_bl_0x5000.bin" -t "Auto Detect" -re on -r 0x10000000 0x10007fff -oe off
cmdwin::fl::erase image
-------------------------
Auto-detection is successful.
File is of type Binary/Raw Format.

Image size is 0 bytes, nothing to erase.
Nothing to erase. No sectors selected
Erase Command Succeeded.
cmdwin::fl::write
-------------------------
Using restricted address range 0x10000000 to 0x10007FFF
Programming file C:\Users\micha\Downloads\0244_k20dx_bl_0x5000.bin
Auto-detection is successful.
File is of type Binary/Raw Format.

0 Bytes Programmed, Check Restricted Address Range
Program Command Succeeded

***************  END of OUTPUT

It seems as though nothing is programmed.  Hints as to what I am doing wrong would be appreciated.

Am I correct in thinking that a USB MSD should appear?  If not, how do I add k20dx_frdmk64f_if_crc_legacy_0x5000.bin  ?

Also,  am  I correct in thinking that if I cut the trace on J11, I can disable the openSDA stuff and use my multilink instead?

Thanks for reading

Michael

标签 (1)
0 项奖励
回复
2 回复数

1,731 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi Michael,

I made a test on my board. Some messages is same as yours. But it really can work. I download the bin file successfully. Below are the photo and screenshot.

After download, re-plug the usb cable, windows will show a new disk named MAINTENANCE. 

1. connection

WeChat Image_20181121135600.jpg

2. setting

cw_prog2.png

3 setting 2(connection edit)

cw_prog3.png

4. context in CW console window

fl::target -lc "LC for Simple Flash (1)"
fl::target -b 0x1fffe000 0x4000
fl::target -v off -l off
cmdwin::fl::device -d "FTFL_PFlash128S1RAM16" -o "32Kx32x1" -a 0x0 0x1ffff
cmdwin::fl::image -f "C:\\Users\\nxf32199\\Documents\\0244_k20dx_bl_0x5000.bin" -t "Auto Detect" -re on -r 0x0 0x1ffff -oe off
cmdwin::fl::erase image
 Beginning Operation ...   
-------------------------
Auto-detection is successful.  
  File is of type Binary/Raw Format.  
 
Performing target initialization ...   
failed on register write: ETF_FCR
 Downloading Flash Device Driver ...  
 Reading flash ID ...
Erasing Sector 0x00000000 to 0x000003FF  
Erasing Sector 0x00000400 to 0x000007FF  
Erasing Sector 0x00000800 to 0x00000BFF  
Erasing Sector 0x00000C00 to 0x00000FFF  
Erasing Sector 0x00001000 to 0x000013FF  
Erasing Sector 0x00001400 to 0x000017FF  
Erasing Sector 0x00001800 to 0x00001BFF  
Erasing Sector 0x00001C00 to 0x00001FFF  
Erasing Sector 0x00002000 to 0x000023FF  
Erasing Sector 0x00002400 to 0x000027FF  
Erasing Sector 0x00002800 to 0x00002BFF  
Erasing Sector 0x00002C00 to 0x00002FFF  
Erasing Sector 0x00003000 to 0x000033FF  
Erasing Sector 0x00003400 to 0x000037FF  
Erasing Sector 0x00003800 to 0x00003BFF  
Erasing Sector 0x00003C00 to 0x00003FFF  
Erasing Sector 0x00004000 to 0x000043FF  
Erasing Sector 0x00004400 to 0x000047FF  
Erasing Sector 0x00004800 to 0x00004BFF  
Erasing Sector 0x00004C00 to 0x00004FFF  
 Erasing ...
 Erase Command Succeeded   
cmdwin::fl::write
 Beginning Operation ...   
-------------------------
Using restricted address range 0x00000000 to 0x0001FFFF  
Programming file C:\Users\nxf32199\Documents\0244_k20dx_bl_0x5000.bin  
Auto-detection is successful.  
  File is of type Binary/Raw Format.  
 
 Downloading Flash Device Driver ...  
 Reading flash ID ...
Auto-detection is successful.  
  File is of type Binary/Raw Format.  
 
Downloading 0x00003310 bytes to be programmed at 0x00000000  
Executing program ....  
 Program Command Succeeded   
Downloading 0x00001CF0 bytes to be programmed at 0x00003310  
Executing program ....  
 Program Command Succeeded   
cmdwin::fl::device -d "FTFL_DFlash32S1RAM16" -o "8Kx32x1" -a 0x10000000 0x10007fff
cmdwin::fl::image -f "C:\\Users\\nxf32199\\Documents\\0244_k20dx_bl_0x5000.bin" -t "Auto Detect" -re on -r 0x10000000 0x10007fff -oe off
cmdwin::fl::erase image
-------------------------
Auto-detection is successful.  
  File is of type Binary/Raw Format.  
 
Image size is 0 bytes, nothing to erase.  
Nothing to erase.  No sectors selected
Erase Command Succeeded.  
cmdwin::fl::write
-------------------------
Using restricted address range 0x10000000 to 0x10007FFF  
Programming file C:\Users\nxf32199\Documents\0244_k20dx_bl_0x5000.bin  
Auto-detection is successful.  
  File is of type Binary/Raw Format.  
 
 0 Bytes Programmed, Check Restricted Address Range  
Program Command Succeeded  

Regards,

Jing

0 项奖励
回复

1,731 次查看
BlackNight
NXP Employee
NXP Employee

>>

Also,  am  I correct in thinking that if I cut the trace on J11, I can disable the openSDA stuff and use my multilink instead?

<<

You can use an external debug probe on the SWD header without cutting the trace on J11. Cutting the trace allows you to use the board to debug an external/other board.

0 项奖励
回复