have the K20 and K24 families the same USB cell? is there the same hw architecture?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

have the K20 and K24 families the same USB cell? is there the same hw architecture?

427 Views
manricoprevital
Contributor I

I have to use a particular (not NXP) USB stack.

I have used this stack for kinesis K20 familiy.

Are the same USB HW cell in the K20 and K24 family?

0 Kudos
Reply
1 Reply

367 Views
miduo
NXP Employee
NXP Employee

Hi,

No, K24_120: USB 2.0 On-The-Go (full-speed) with USB transceiver.

K20_120: USB 2.0 On-The-Go (full and high speed).Current/time for portable USB devices enabling longer battery life. 

So they are different.

0 Kudos
Reply