I have a FRDM_64 board. And I have been trying to get frdmk66f_lwip_udpecho_bm.c to run. When I go to debug it seems to stop on line 95 of lwip_udpecho_bm.c (BOARD_BootClockRUN();). Thread 1 is running.
My PC's IP port is set to is configured as 192.168.0.100. The debug window shows:
main () at ../source/lwip_udpecho_bm.c:87
87 ethernetif_config_t fsl_enet_config0 = {
Program received signal SIGTRAP, Trace/breakpoint trap.
0x0000c7ba in HardFault_Handler () at ../source/semihost_hardfault.c:72
72 __asm( ".syntax unified\n"
tbreak main
Note: breakpoint 8 also set at pc 0x50e.
Temporary breakpoint 10 at 0x50e: file ../source/lwip_udpecho_bm.c, line 87.
monitor reset
continue
Continuing.
Temporary breakpoint 8, main () at ../source/lwip_udpecho_bm.c:87
87 ethernetif_config_t fsl_enet_config0 = {
No breakpoint number 10.
Program received signal SIGINT, Interrupt.
main () at ../source/lwip_udpecho_bm.c:87
87 ethernetif_config_t fsl_enet_config0 = {
The console shows:
SEGGER J-Link GDB Server V6.44f - Terminal output channel
Resetting target
Resetting target
Resetting target
Resetting target
--------------------------------------------------------------
C:\Users\Randy\Downloads\EchoTool-master\EchoTool-master\EchoTool\bin\Debug>echo
tool 192.168.0.102 /p udp /r 7 /d hello
Hostname 192.168.0.102 resolved as 192.168.0.102
Response time out
Response time out
Response time out
Response time out
Response time out
Statistics: Received=0, Corupted=0, Lost=5
C:\Users\Randy\Downloads\EchoTool-master\EchoTool-master\EchoTool\bin\Debug>
解決済! 解決策の投稿を見る。
K66's code can't run on K64. Their MCG block are different. They are different device. Please download FRDM-K64F SDK and try frdmk64f_lwip_udpecho_bm.
Regards,
Jing
Jing Pan:
Yes, you are correct. It works now. Thanks.
Randy
Hi,
Since your code stops on BOARD_BootClockRUN() and hardfault happen, I think there may be some clock setting error. At this stage, lwip even doesn't initialized. Do you change the clock setting? If yes, you can re-config clock tree at ConfigTools->clocks. This tool make the work visualize and it can check the result.
If the problem still there, please show me how you config the clock.
Regards,
Jing
I did not change the clock. It is the same as the initial install.
Hi,
You use frdmk66f_lwip_udpecho_bm as demo, but your board is frdm-k64?
Yes, I am using FRDM-k64 for this demo. How can I check the clock's setting in ConfigTools->clocks ? What should its
setting be normally ?