I have been working with frdmk64f_lwip_tcpecho_bm. It worked at first, then I changed the IP address and now I get:
C:\Users\Randy\Downloads\EchoTool-master\EchoTool-master\EchoTool\bin\Debug>ech
otool 192.168.1.129 /p tcp /r 7 /d hello
Hostname 192.168.1.129 resolved as 192.168.1.129
Can not connect to server
Statistics: Received=0, Corrupted=0
C:\Users\Randy\Downloads\EchoTool-master\EchoTool-master\EchoTool\bin\Debug>
Any ideas what I am doing wrong ?
Well I started over with this. I deleted the my original example, I imported the example again, the ip address is 192.168.0.102 , the subnet mask is 192.168.0.102, and when I try to run the example I get:
C:\Users\Randy\Downloads\EchoTool-master\EchoTool-master\EchoTool\bin\Debug>echo
tool 192.168.0.102 /p tcp /r 7 /d hello
Hostname 192.168.0.102 resolved as 192.168.0.102
Can not connect to server
Statistics: Received=0, Corrupted=0
C:\Users\Randy\Downloads\EchoTool-master\EchoTool-master\EchoTool\bin\Debug>
Any ideas ?
One additional note is that you can ping the board and it will reply.
C:\Users\Randy>ping 192.168.0.102
Pinging 192.168.0.102 with 32 bytes of data:
Reply from 192.168.0.102: bytes=32 time<1ms TTL=128
Reply from 192.168.0.102: bytes=32 time<1ms TTL=128
Reply from 192.168.0.102: bytes=32 time<1ms TTL=128
Reply from 192.168.0.102: bytes=32 time<1ms TTL=128
Ping statistics for 192.168.0.102:
Packets: Sent = 4, Received = 4, Lost = 0 (0% loss),
Approximate round trip times in milli-seconds:
Minimum = 0ms, Maximum = 0ms, Average = 0ms
C:\Users\Randy>
Hi Randy:
If you change the echo server ip address, please make sure change your PC's ip address too to make sure they are in the same subnet.
I did a quick check on my side, it is OK.
Regards
Daniel