firmware upgradation over Air

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

firmware upgradation over Air

1,016 次查看
mayursavaj
Contributor III

Hi All,

I am working as firmware Developer. We are working on Cortex M4 Series micro controller (MK22Fx512).

Is there any method to upgrade firmware over the Air? Our device have GPRS Connectivity.

Thanks in advance.

标签 (1)
0 项奖励
回复
1 回复

786 次查看
Rick_Li
NXP Employee
NXP Employee

Hi Mayur Savaj,

the below is the link for AN2295 which is on developing a serial bootloader.

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295.pdf

you can also download the corresponding SW for AN2295 by searching AN2295SW in Freescale website.

Here suppose your GPRS module is connected to MK22 by using a serial port.

if you can reset the MCU, then, by transfer data via GPRS, you may update the firmware.

I hope it helps!

0 项奖励
回复