I am in the process of setting up emWin to run on a custom board (custom bsp) with MK22FX512AVLQ12 MCU.
There appears to be a library call "APPW_Init()" that is found in APPMainTask.c for most BSP examples that use emWin 6.10f along with AppWizard:
"...
void MainTask(void) {
//
// Setup configuration dependent pointers
//
APPW_X_Setup();
//
// Initialize AppWizard
//
APPW_Init(APPW_PROJECT_PATH);
//
// Create initial screen...
//
APPW_CreateRoot(APPW_INITIAL_SCREEN, WM_HBKWIN);
..."
Is the APPW_Init() needed when compiling AppWizard in my custom board project?
What happens if APPW_Init() is commented out (or not used)?
What resource files from "APPW_PROJECT_PATH" are accessed when App_Init() is called?
已解决! 转到解答。
Hi lsrbigfoot,
APPW_Init is necessary for any AppWizard project. It initializes and configures the GUI as well as initializes the text usage. If a file system is being used, it will also initialize that. If you try to comment this out, you will get a hard fault (this is what happened in my system).
APPW_PROJECT_PATH is only utilized when running the AppWizard simulator.
Best regards,
Chris
Hi lsrbigfoot,
APPW_Init is necessary for any AppWizard project. It initializes and configures the GUI as well as initializes the text usage. If a file system is being used, it will also initialize that. If you try to comment this out, you will get a hard fault (this is what happened in my system).
APPW_PROJECT_PATH is only utilized when running the AppWizard simulator.
Best regards,
Chris