Hello,
I'm unable to pass calibration procedure (D4D_CalibrateTouchScreen()). My touch screen controller is cr touch (d4dtch_cr_touch.c version 0.0.4.0, date Nov-24-2011). When I touch yellow cross, I get {25, 25} {124, 250} {225, 450} coordinates on the screen (that seems fine), but the code never passes
if ((X[0] > X[1]) && (X[1] > X[2]) && (Y[0] > Y[1]) && (Y[1] > Y[2])) // line 775 in d4d_low.c, version 0.0.43.0, date Feb-23-2011
How should I configure D4D or cr touch to pass the calibration procedure?
Thanks
Martin
已解决! 转到解答。
Hello,
You need to call periodically D4D_CheckTouchScreen();
In the eGUI examples, this is done using PIT timer interrupt. You can mantain some timing flags to be used in your application. This is the typical code:
/**************************************************************//*!
* Periodic IRQ callback or IRQ function
******************************************************************/
void pit_ch0_callback(void)
{
static Byte actual_time = 0;
TIME_FLAGS flags;
actual_time++;
flags.all = (LWord)(actual_time ^ (actual_time - 1));
time.all |= flags.all;
if(flags.bits.b50ms)
{
// Key_CheckKeys();
D4D_CheckTouchScreen();
}
D4D_TimeTickPut();
if(flags.bits.b100ms)
{
time100sm_cnt++;
}
}
The flags definition:
// typedef definitions
typedef union
{
LWord all;
struct
{
unsigned b25ms :1;
unsigned b50ms : 1;
unsigned b100ms : 1;
unsigned b200ms : 1;
unsigned b400ms : 1;
unsigned b800ms : 1;
unsigned b1600ms : 1;
unsigned b3200ms : 1;
}bits;
}TIME_FLAGS;
// global variables externs
extern TIME_FLAGS time;
extern LWord time100sm_cnt;
Best Regards,
Luis
OK, now I can pass the calibration procedure.
However, I have another problem - after the calibration is done, my application doesn't receive any touches. The function "D4DTCH_GetPositionRaw_CrTouch() - d4dtch_cr_touch.c" is never called from that moment.
I call D4D_Poll in my main application loop.
Hello,
You need to call periodically D4D_CheckTouchScreen();
In the eGUI examples, this is done using PIT timer interrupt. You can mantain some timing flags to be used in your application. This is the typical code:
/**************************************************************//*!
* Periodic IRQ callback or IRQ function
******************************************************************/
void pit_ch0_callback(void)
{
static Byte actual_time = 0;
TIME_FLAGS flags;
actual_time++;
flags.all = (LWord)(actual_time ^ (actual_time - 1));
time.all |= flags.all;
if(flags.bits.b50ms)
{
// Key_CheckKeys();
D4D_CheckTouchScreen();
}
D4D_TimeTickPut();
if(flags.bits.b100ms)
{
time100sm_cnt++;
}
}
The flags definition:
// typedef definitions
typedef union
{
LWord all;
struct
{
unsigned b25ms :1;
unsigned b50ms : 1;
unsigned b100ms : 1;
unsigned b200ms : 1;
unsigned b400ms : 1;
unsigned b800ms : 1;
unsigned b1600ms : 1;
unsigned b3200ms : 1;
}bits;
}TIME_FLAGS;
// global variables externs
extern TIME_FLAGS time;
extern LWord time100sm_cnt;
Best Regards,
Luis
Hi,
I'm using eGUI v2.07; I have same problem with you when I do calibration. I use TSC2046 touch driver, I always get: X1 > X2 > X3 but Y1 < Y2 < Y3.
Then I try to revert Y axis to pass calibration phase (#define D4DTCH_AXIS_ORIENT_Y D4DTCH_AXIS_ORIENT_INVERTED), when go in the display, I can not touch exactly on the button (play, stop, menu).
Thanks,
Vu Phung
Hi Martin,
To do calibration ok, I think you just revert X,Y axis as your result You show. Ex:
#if D4DTCH_AXIS_ORIENT_Y == D4DTCH_AXIS_ORIENT_INVERTED
tmpRes = (unsigned short)(D4DTCH_FULL_SCALE - tmpRes);
#endif
BTW, I have fixed my problem. My problem is that X+/X- & Y+/Y- of touch panel is connected crossly with X+/X- & Y+/Y- of TSC2046. So in the source code, just swap x, y value.