differences bewteen k53 k60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

differences bewteen k53 k60

1,885 Views
ednasalazar
Contributor II

Hi everbody,

I developped SPI, UART I2C, interfaces using TWR-K60N512, however if i try to change of µC (K53) using TWR K53 it doesnt work.

Can somebody explain me what is it the difference between both µC?

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,699 Views
ivadorazinova
NXP Employee
NXP Employee

Hi edna salazar,


please, can you specify what does not work?

TWR-K60N512 and TWR-K53N512 are similar devices.


Both of them have 3x SPI modules, 2x I2C modules, 6x UART modules, SDHC and I2S module communication interface.

TWR-K60N512 has Two Controller Area Network (CAN) modules in difference with TWR-K53N512.


So, it should works.


I attach you the comparison.

hw.png

You can try our Product Selector Freescale Product Selector


Best Regards,

Iva




1,699 Views
ednasalazar
Contributor II

Hello Iva,

Thank you very much for your help.

However I found that the main difference between  both µC is the clock configuration and the clock associated with each module.

0 Kudos
Reply