converter from CAN to UART

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

converter from CAN to UART

2,838 次查看
kentgu
Contributor III

hi, If Freescal have one chip, can realize convter CAN bus to UART, it don' need to program. TKS~ Kent

0 项奖励
回复
2 回复数

1,838 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Kent,

Please go ahead to find some information about the CAN transceivers through the link as below.

CAN Physical Interfaces|Freescale
Have a great day,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,838 次查看
kentgu
Contributor III

Hi Jerremy,

Yes, you are right. we can use CAN transciever. but it just realize to CANRx, CANTx signal to differentiial signal. can't convert CAN protocol to UART protco..

TKS~

Kent

0 项奖励
回复