converter from CAN to UART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

converter from CAN to UART

2,843 Views
kentgu
Contributor III

hi, If Freescal have one chip, can realize convter CAN bus to UART, it don' need to program. TKS~ Kent

0 Kudos
Reply
2 Replies

1,843 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Kent,

Please go ahead to find some information about the CAN transceivers through the link as below.

CAN Physical Interfaces|Freescale
Have a great day,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,843 Views
kentgu
Contributor III

Hi Jerremy,

Yes, you are right. we can use CAN transciever. but it just realize to CANRx, CANTx signal to differentiial signal. can't convert CAN protocol to UART protco..

TKS~

Kent

0 Kudos
Reply