Hi,
MCU----->MKL16z64vlh4
Aim------>Upgrade my firmware through Low power uart
I have checked the kinetis bootloader part and found out my mcu wont support Boot Rom,going further i understood there is some way to port the kinetis bootloader(Time consuming ??) ....so i was searching for some sample code in keil for kl16 series that i can copy and edit to do my application,unfortunately i didn't find anything.... can any one help me with this.....................??? and is there any way to open code-warrior project in keil ?????
已解决! 转到解答。
Hello sachin,
We have one bootloader for kl26 through UART , and include the KEIL version . It will be published on the web soon.
Now i send it to you by attachment .
I think it is easy to porting it to KL16 .
In the attachment , you can fund the KEIL version on :
"Kinetis-Bootloader-master1027\Kinetis Bootloader SW\Bootloader and Application for KL26\Bootloader Source Code\boorloader_kl26_MDK "
And about the Reference manual you can fund here :
Kinetis-Bootloader-master1027\Kinetis-Bootloader-master1027\Kinetis Bootloader DOC - 0915.pdf .
(This RM is refer to the CW version , while you can refer to ).
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Alice
Hello sachin,
We have one bootloader for kl26 through UART , and include the KEIL version . It will be published on the web soon.
Now i send it to you by attachment .
I think it is easy to porting it to KL16 .
In the attachment , you can fund the KEIL version on :
"Kinetis-Bootloader-master1027\Kinetis Bootloader SW\Bootloader and Application for KL26\Bootloader Source Code\boorloader_kl26_MDK "
And about the Reference manual you can fund here :
Kinetis-Bootloader-master1027\Kinetis-Bootloader-master1027\Kinetis Bootloader DOC - 0915.pdf .
(This RM is refer to the CW version , while you can refer to ).
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Alice
Thanks Alice ,,,
I have one more question regarding this,,,,kl26 have 128kb flash and kl16z64 have only 64kb, does this cause any problem ...what all things i should edit in it to make it kl16 IC...
Hello sachin,
About change , it mainly include two parts:
- The first part is bootloader code :
- the UART port ;
- the flash , especially the "APPOK_START_ADDRESS", it defined in the file of "FRDM_KL26Z_cfg.h":
| #define APPOK_START_ADDRESS | 0x1FFF8 |
for your chip is 64k size flash , here you need change it to 0xFFF8 .
and other about flash need to be change , please refer to this picture to check whether is right :
- The other part is the GUI code : mainly change the file of ""GlobalVars.cs" ,
you need refer to the "MKL26128" to add other part as it :
You can first change the places i mentioned above , then test , if it sitll can not work , you can tell me the detail information or
which step it failed , then i will check with you .
Furthermore , if you use the keil , you only need check these folders :
-Kinetis-Bootloader-master\ Kinetis-Bootloader-master1027\Kinetis Bootloader SW\Bootloader and Application for KL26\Bootloader Source Code\boorloader_kl26_MDK
- Kinetis-Bootloader-master\Kinetis-Bootloader-master1027\Kinetis Bootloader SW\Bootloader GUI Source Code\Boot_Loader_GUI 20151026
- Kinetis-Bootloader-master\Kinetis-Bootloader-master1027\Kinetis Bootloader SW\Bootloader and Application for KL26\User Application Source Code (this are app code created on CodeWarrior)-
- Kinetis-Bootloader-master\Kinetis-Bootloader-master1027\Kinetis Bootloader DOC - 0915.pdf (This DOC is detail about the bootloader , i recommend you check it )
Hope it helps
Alice
Hi Alice,
Thanks for the replay.. now iam able to write into flash but i am not able to jump to user program after writing.
Function ::
void JumpToUserApplication(LWord userSP, LWord userStartup)
{
volatile LWord avoid_optimization;
avoid_optimization = userSP; //In order to avoid optimization issue when -Os
avoid_optimization = userStartup; //In order to avoid optimization issue when -Os
// set up stack pointer
__asm("msr msp, r0");
__asm("msr psp, r0");
// Jump to PC (r1)
__asm("mov pc, r1");
}
is showing error ,,,,,,,,,,......
compiling bootloader.c...
..\Sources\bootloader.c(110): warning: #1267-D: Implicit physical register R0 should be defined as a variable
__asm("MSR MSP, R0");
..\Sources\bootloader.c(110): error: #549: variable "R0" is used before its value is set
__asm("MSR MSP, R0");
..\Sources\bootloader.c(114): error: #20: identifier "PC" is undefined
__asm("MOV PC, R1");