Will there be a Freedom board for Kinetis K50, K51 or K53 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Will there be a Freedom board for Kinetis K50, K51 or K53 ?

870 Views
chadwilliams
Contributor III

I have looked at the Kinetis K50, K51 & K53 processors and they appear to be a good match for

instrumentation applications which is my area of interest.

The 16 bit ADC's with PGA's and the onboard Opamps and DAC's  would be very useful

in producing low component count / low cost products.

However I have not been successful in finding a selection of evaluation boards for this

series other than the Tower Module TWR-K53n512 which uses the high end K53 in a BGA package.

There is some modules such as the MED-EKG module that can plug into the TWR-K53

but there is no FRDM-K50 or FRDM-K51.

Will there be more boards in future based on this series ?

0 Kudos
1 Reply

384 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Chad:

Unfortunately right now there are no plans for a freedom board or other board for K5x devices. The option is the tower system and in particular the board you mentioned, TWR-K53N512.

The available enablement software is listed in your other question: When will TWR-K53n512 be supported by KDS and KSDK?


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------