Will K22 meet MFi lower power requirements?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Will K22 meet MFi lower power requirements?

661件の閲覧回数
ChrisDarrow
Contributor III

Can a measurement on the K22 be done with the Vbus at 3.3V as is required by MFi? There are actually two power modes required:

  1. Low Power mode: the device is not running an audio app, has told the accessory to reduce current draw below 10mA & enter the zero bandwidth configuration, meaning that the device is still sending USB data frames & the accessory should be able to rapidly wake up when the relevant wake command is given.
  2. High Power mode: the device is now running an audio app & streaming audio data. The accessory must draw less than 100mA. The measurement in this mode is complicated, but I'll just boil it down to the bottom line that we need the MCU to come in at about 30mA or less here to make our system compliant.

Has Freescale measured the K22 for MFi applications? Can it meet the above requirements? Ideally do you have a demo app I can run on the FRDM-K22F to measure the two scenarios above to determine if the K22 is compliant for power consumption?

Thanks,

Chris

ラベル(1)
0 件の賞賛
2 返答(返信)

566件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Chris,

this information is only provided under NDA. Please enter a ticket at www.nxp.com/support

You will see at the bottom "Submit new tickets" section and you may select Hardware & Software

Regards,

Carlos

0 件の賞賛

566件の閲覧回数
ChrisDarrow
Contributor III

Some additional information and request:

Accessory Interface Spec from Apple for MFi - section 28.2.1 - states that the device transitioning from the streaming interface to the zero bandwidth interface should be used as the trigger for the accessory to transition form high to low power modes. There doesn't seem to be any mention of any USB suspend, wait or stop modes as an option to trigger power mode transition. Is there any demo code to help with this?

0 件の賞賛