Why is TWR-K20D72M not supported in MCUxpresso !?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why is TWR-K20D72M not supported in MCUxpresso !?

Jump to solution
683 Views
dirk_uhlemann
Contributor I

Why is this Dev.-Board and the Chip   K20DX256VLL7  not supported? 

I found only the K20DX256xxx10  as supported device.

So is there a Workaround to use the K20DX256VLL7 anyway?

I am using V 10.2  of this IDE

Regards,
Dirk Uhlemann

Labels (1)
0 Kudos
Reply
1 Solution
592 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Dirk:

Unfortunately MK20DX256VLH7 is not supported in MCUXpresso SDK. There is no guider or work around to port it from an existing SDK. 

If you use the other similar SDK to run the specified chips, it is possibly that you may encounter issues because there maybe difference between IPs IN 100M and 72M. And NXP support can't help on this.

You can download the bare metal code examples from below link

TWR-K20D72M|Tower System Board|Kinetis MCUs|NXP 

Or you can use Classic MQX 4.2 (free) , TWR-K20D72M is supported.

Regards

Daniel

View solution in original post

0 Kudos
Reply
1 Reply
593 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Dirk:

Unfortunately MK20DX256VLH7 is not supported in MCUXpresso SDK. There is no guider or work around to port it from an existing SDK. 

If you use the other similar SDK to run the specified chips, it is possibly that you may encounter issues because there maybe difference between IPs IN 100M and 72M. And NXP support can't help on this.

You can download the bare metal code examples from below link

TWR-K20D72M|Tower System Board|Kinetis MCUs|NXP 

Or you can use Classic MQX 4.2 (free) , TWR-K20D72M is supported.

Regards

Daniel

0 Kudos
Reply